GANTRY.PL.ERRWTHRESH

Description

If this value does not equal 0 and the position error GANTRY.PL.ERR is larger than this value, the drive will generate a warning.

If GANTRY.PL.ERRWTHRESH is set to 0 the warning is not issued.

Versions

Action Version Notes
Implemented 02-02-02-000  

General Information

Type Read/Write
Description Sets the position error warning level for Gantry Mode.
Units

Rotary: counts, rad, deg, custom units, 16-bit counts

Linear: counts, mm, µm, custom units, 16-bit counts

See Position Units for details.

Range Depends on units. See Position Range for details.
Default Value 0 counts
Data Type Float
See Also AXIS#.PL.FB
Stored in Non-Volatile Memory Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

GANTRY.PL.ERRWTHRESH

300eh

03h

Signed32

Position

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

3002

1

3002 (0xbba)

GANTRY.PL.ERRWTHRESH

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

GANTRY.PL.ERRWTHRESH

3002

Signed32

Read/Write

Position